Red State Machine file generator: Action List bug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Red State Machine file generator: Action List bug

1,357 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntorresa on Sat Apr 05 00:47:14 MST 2014
Hello, I can add actions and operations:

[img=279x168]http://i.imgur.com/rmjPPXw.jpg[/img]

But when I click on SET to change the Value field, the Operation simply dissapears:

[img=280x171]http://i.imgur.com/fBein1b.jpg[/img]

I'm using LPCXpresso v7.1.1 [Build 125].
0 Kudos
Reply
4 Replies

1,332 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntorresa on Mon Apr 07 20:42:46 MST 2014
I am not using a SCT state machine, I am using a software state machine.
0 Kudos
Reply

1,332 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Apr 07 17:33:00 MST 2014
Hi ntorresa,
LPC175x_6x does not contain SCTimer block. Could you please try any of below devices?
LPC1800
LPC4300
LPC1500
LPC11U6x
LPC1800

Please post your result if you still see bug.
0 Kudos
Reply

1,332 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ntorresa on Mon Apr 07 12:34:10 MST 2014
Thanks for your reply Joe.

Test scenario: Switch to a new workspace, create a new C project for LPC175x_6x using CMSIS_CORE_LPC17xx and add a software state machine. Open the .rsm file and add with the + button a new output and a new action. Select the action, right click on the operation list > set > output 1. Click on SET to be able to change the value field and it dissapears. Restart LPCXpresso, the bug is still there.

I am using Windows 8.1.

Regards.
0 Kudos
Reply

1,332 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JoeHale on Mon Apr 07 07:37:03 MST 2014
Hi,

Thanks for bringing this issue to our attention. I am having trouble reproducing the bug though. I'm assuming that you are using the software state machine functionality.

I have a couple of questions for you:

[list]
  [*] Are you able to reproduce it after restarting LPCXpresso?
  [*] What operating system are you using?
  [*] How did you add the action - using the + button, the context menu in the action list, the state table or the state diagram?
[/list]

Thanks,

Joe Hale
0 Kudos
Reply