Recreate Example001 from FreeRTOS manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recreate Example001 from FreeRTOS manual

1,133 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mwoodmansee on Mon Jul 29 18:41:42 MST 2013
I am trying to learn about the LPC1769 and am rewriting the examples used in Richard Barry's FreeRTOS manual.  When I compile a retyped version of Example01 called example01_rework I get the following compilation dump. 

Please provide your thoughts.


****************************************************************************************
20:28:54 **** Incremental Build of configuration Debug for project example01_rework ****
make all
Building file: ../src/cr_startup_lpc17.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"src/cr_startup_lpc17.d" -MT"src/cr_startup_lpc17.d" -o "src/cr_startup_lpc17.o" "../src/cr_startup_lpc17.c"
Finished building: ../src/cr_startup_lpc17.c

Building file: ../src/main.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"src/main.d" -MT"src/main.d" -o "src/main.o" "../src/main.c"
../src/main.c: In function 'main':
../src/main.c:38:2: warning: implicit declaration of function 'printf' [-Wimplicit-function-declaration]
../src/main.c:41:2: warning: pointer targets in passing argument 2 of 'xTaskGenericCreate' differ in signedness [-Wpointer-sign]
../FreeRTOS_include/task.h:1299:22: note: expected 'const signed char * const' but argument is of type 'char *'
../src/main.c:49:2: warning: pointer targets in passing argument 2 of 'xTaskGenericCreate' differ in signedness [-Wpointer-sign]
../FreeRTOS_include/task.h:1299:22: note: expected 'const signed char * const' but argument is of type 'char *'
../src/main.c: At top level:
../src/main.c:23:13: warning: 'setupHardware' defined but not used [-Wunused-function]
Finished building: ../src/main.c

Building file: ../FreeRTOS_src/croutine.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_src/croutine.d" -MT"FreeRTOS_src/croutine.d" -o "FreeRTOS_src/croutine.o" "../FreeRTOS_src/croutine.c"
Finished building: ../FreeRTOS_src/croutine.c

Building file: ../FreeRTOS_src/list.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_src/list.d" -MT"FreeRTOS_src/list.d" -o "FreeRTOS_src/list.o" "../FreeRTOS_src/list.c"
Finished building: ../FreeRTOS_src/list.c

Building file: ../FreeRTOS_src/queue.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_src/queue.d" -MT"FreeRTOS_src/queue.d" -o "FreeRTOS_src/queue.o" "../FreeRTOS_src/queue.c"
Finished building: ../FreeRTOS_src/queue.c

Building file: ../FreeRTOS_src/tasks.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_src/tasks.d" -MT"FreeRTOS_src/tasks.d" -o "FreeRTOS_src/tasks.o" "../FreeRTOS_src/tasks.c"
Finished building: ../FreeRTOS_src/tasks.c

Building file: ../FreeRTOS_src/timers.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_src/timers.d" -MT"FreeRTOS_src/timers.d" -o "FreeRTOS_src/timers.o" "../FreeRTOS_src/timers.c"
Finished building: ../FreeRTOS_src/timers.c

Building file: ../FreeRTOS_portable/MemMang/heap_2.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_portable/MemMang/heap_2.d" -MT"FreeRTOS_portable/MemMang/heap_2.d" -o "FreeRTOS_portable/MemMang/heap_2.o" "../FreeRTOS_portable/MemMang/heap_2.c"
Finished building: ../FreeRTOS_portable/MemMang/heap_2.c

Building file: ../FreeRTOS_portable/port.c
Invoking: MCU C Compiler
arm-none-eabi-gcc -D__NEWLIB__ -DDEBUG -D__CODE_RED -DPACK_STRUCT_END=__attribute\(\(packed\)\) -DGCC_ARMCM3 -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\FreeRTOS_Library\demo_code" -I"C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\CMSISv1p30_LPC17xx\inc" -I../src -I../FreeRTOS_include -I../FreeRTOS_portable -O0 -g3 -Wall -c -fmessage-length=0 -fno-builtin -ffunction-sections -fdata-sections -mcpu=cortex-m3 -mthumb -MMD -MP -MF"FreeRTOS_portable/port.d" -MT"FreeRTOS_portable/port.d" -o "FreeRTOS_portable/port.o" "../FreeRTOS_portable/port.c"
Finished building: ../FreeRTOS_portable/port.c

Building target: example01_rework.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -Xlinker -Map="example01_rework.map" -Xlinker --gc-sections -mcpu=cortex-m3 -mthumb -T "example01_rework_Debug.ld" -o "example01_rework.axf"  ./src/cr_startup_lpc17.o ./src/main.o  ./FreeRTOS_src/croutine.o ./FreeRTOS_src/list.o ./FreeRTOS_src/queue.o ./FreeRTOS_src/tasks.o ./FreeRTOS_src/timers.o  ./FreeRTOS_portable/MemMang/heap_2.o  ./FreeRTOS_portable/port.o  
./src/main.o: In function `vTask1':
C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\example01_rework\Debug/../src/main.c:71: undefined reference to `vPrintString'
./src/main.o: In function `vTask2':
C:\Users\h117018\Documents\LPCXpresso_5.2.6_2137\workspace\example01_rework\Debug/../src/main.c:93: undefined reference to `vPrintString'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-sbrkr.o): In function `_sbrk_r':
sbrkr.c:(.text._sbrk_r+0xc): undefined reference to `_sbrk'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-writer.o): In function `_write_r':
writer.c:(.text._write_r+0x10): undefined reference to `_write'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-closer.o): In function `_close_r':
closer.c:(.text._close_r+0xc): undefined reference to `_close'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-fstatr.o): In function `_fstat_r':
fstatr.c:(.text._fstat_r+0xe): undefined reference to `_fstat'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-isattyr.o): In function `_isatty_r':
isattyr.c:(.text._isatty_r+0xc): undefined reference to `_isatty'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-lseekr.o): In function `_lseek_r':
lseekr.c:(.text._lseek_r+0x10): undefined reference to `_lseek'
c:/nxp/lpcxpresso_5.2.6_2137/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.6.2/../../../../arm-none-eabi/lib/armv7-m\libc.a(lib_a-readr.o): In function `_read_r':
readr.c:(.text._read_r+0x10): undefined reference to `_read'
collect2: ld returned 1 exit status
make: *** [example01_rework.axf] Error 1

20:29:04 Build Finished (took 9s.773ms)

0 Kudos
Reply
1 Reply

896 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Jul 29 23:34:13 MST 2013
I think this FAQ from Code Red will help.

http://support.code-red-tech.com/CodeRedWiki/UndefinedReference
0 Kudos
Reply