Reading USB Mass storage devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reading USB Mass storage devices

845 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bhallett on Wed Feb 03 04:17:35 MST 2010
Hello all,

Does anyone know/think if/it is possible to program the lpc1342 device to read  the contents of a mass storage device rather than a lpc1342 becoming a mass storage device?

Regards

Barry
0 项奖励
回复
2 回复数

831 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Wed Feb 03 08:27:23 MST 2010
Although you can't directly connect a usb mass storage device, you ought to be able to connect the SSP/SPI up to an SD card, which might provide the functionality you are after.
0 项奖励
回复

831 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by annodomini2 on Wed Feb 03 05:41:08 MST 2010
The USB interface on the LPC1343 is Device level only, so no as far as I am aware.

You would need an LPC17xx series with Host and/or OTG support.
0 项奖励
回复