Re LPCXpresso (free) Code Size Limit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re LPCXpresso (free) Code Size Limit

1,489件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Sep 20 20:14:44 MST 2012
[SIZE=2][FONT=Tahoma]To summarise: Can the free IDE debug code larger than the 128K limit providing that any flash loading (by the debugger) is not attempted?
   
  [/FONT][/SIZE][SIZE=2][FONT=Tahoma]I fully understand the download size limitation with the free version of the LPCXpresso IDE.

I am using a (custom) boot loader scenario where the boot loader is only 8K or so which programs application code (potentially larger than 128K) into a separate area of flash.

Is is still possible to use the free version of LPCXpresso to debug this large application in flash provided that the launch config option 'load' is false. I.e. if I do not attempt to use the IDE to program the separate appliction?

[I have seen the FAQ page about debugging through a boot loader.]

Cheers, Mike
[/FONT][/SIZE]
0 件の賞賛
返信
3 返答(返信)

1,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Sep 21 09:10:54 MST 2012

Quote: MikeSimmonds

Are the larger (paid for) IDE's exactly the same version as the free, but with bigger allowances?



No - they have more functionality, such as Red Trace, as well as larger code sizes.

A good starting point for more information is...

http://support.code-red-tech.com/CodeRedWiki/ProductOverview

plus the product comparison table at...

http://www.code-red-tech.com/products.php#comparison


Regards,
CodeRedSupport
0 件の賞賛
返信

1,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Sep 21 08:25:24 MST 2012
[SIZE=2][FONT=Tahoma]Thanks for the clarification.

Are the larger (paid for) IDE's exactly the same version as the free, but with bigger allowances?

[/FONT][/SIZE]
0 件の賞賛
返信

1,391件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Sep 21 00:39:21 MST 2012
No. The 128k limit if for download and debug.
0 件の賞賛
返信