RDB1768v2 with LPCXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RDB1768v2 with LPCXpresso

964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giamby3000 on Tue Jan 31 07:00:11 MST 2012
Hi. A simple question: is it possible to use RDB1768v2 Evaluation board with LPCXpresso in order to program flash of my target boards?
Have I to use RDB1768v2 J2 SWO connector? Does it work? On RDB1768 schematic J2 is indicate as Production / Test only: so can I use it?
Can I use RDB1768vs board instead of LPCLink  throught J2 Jtag connector??


Thanks
0 件の賞賛
返信
3 返答(返信)

954件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jan 31 07:37:07 MST 2012
No, you cannot do this.
0 件の賞賛
返信

954件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giamby3000 on Tue Jan 31 07:35:46 MST 2012
Sorry but your link doesn't answer my question. I don't want to use LPCXpresso board (i.e. LPC Link separated from LPC11xx target) but I want to use LPC1758 on RDB1768v2 board (see http://support.code-red-tech.com/CodeRedWiki/RDB1768V2Support ) to program my target boards, but I don't find how can I do it. On this board there is a J2 connector that gets Jtag signal but I don't understand if it is driven or not. J1 is use for program LPC1768 on RDB1768v2 with Code Red Trace.or  probe.
Have you got an idea?
0 件の賞賛
返信

954件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jan 31 07:17:25 MST 2012
Did you try a search already :rolleyes:

http://knowledgebase.nxp.com/showthread.php?t=635
0 件の賞賛
返信