[RDB1768cmsis_usb_bootloader.axf] Error 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[RDB1768cmsis_usb_bootloader.axf] Error 1

1,524 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Jul 26 00:51:25 MST 2011
LPC1758 - LpcXpresso 3.6.2
If I compile in debug mode, all is OK, when switch to Release version i have the error in object.
Can help me ?

Thanks
0 Kudos
Reply
5 Replies

1,514 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Jul 26 01:52:09 MST 2011
Sorry all, I have forget to compile in release mode the lcd lib !!!!
Really stupid !!
0 Kudos
Reply

1,514 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jul 26 01:38:00 MST 2011
If you are building one project for release, you have to build all the dependent (library) projects for release too. i.e. build the library project RDB1768cmsis_usbstack for Release.
0 Kudos
Reply

1,514 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Jul 26 01:33:31 MST 2011
OK, I have update my lpcxpressto to 4.0.5 version, but the probelem remain !!
0 Kudos
Reply

1,514 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Tue Jul 26 01:07:21 MST 2011
Hm,

Good to see it's already fixed.
it still is a strange error directing to standard LPCXpresso includes.

I see you are still using the 3.3 version of the tools.
You should have a look at the latest (4.0.5) version. This version is much nicer than the 3.x version but not that different.
The 4.0 version has the new CMSIS 2.0 version, support for the latest lpc1xxx controllers (of course you don't need those when using your 1768 board), some new project wizard (I love the FreeRTOS project) and all kinds of bug fixes.
You will also find a lot of updated examples from both NXP and Code Red.

You can install and use the 4.0.5 version together with your 3.3 version. So there is no risk of getting stuck with a non working system.
But just in case ... export your projects from LPCXpresso 3.3 and import them into a new workspace in 4.0.5. Once you open a 3.3 workspace in 4.0.5 the project files will be updated and I think (almost sure) that this might be a problem when trying to open then with version 3.3 afterwards.

Regards,
[INDENT]Rob
[/INDENT]
0 Kudos
Reply

1,514 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by blasiis on Tue Jul 26 00:56:18 MST 2011
Problem solved, sorry but I have forget to compile a library :-(
0 Kudos
Reply