RAM location for LPC1517 RAM3 is wrong

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAM location for LPC1517 RAM3 is wrong

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdupre on Wed Aug 19 15:56:30 MST 2015
Re: LPCXpresso v7.9.0

I'm looking at the MCU settings for the LPC1517, and it indicates that Ram2_4 (Alias RAM3) starts at 0x2004000.

Where is it getting this information?  According to the user manual, the third bank starts at 0x2002000, right after the second RAM bank.

Bug?


- Joe

0 Kudos
Reply
1 Reply

654 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Aug 19 16:07:58 MST 2015
See:

https://www.lpcware.com/content/forum/ram-sections
0 Kudos
Reply