Question regarding release building & UART bug issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question regarding release building & UART bug issue

884件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Techys on Sat Mar 06 07:31:24 MST 2010
Hi. I'm new to ARM and have been testing things around. I've been testing around with a LPC1343. I tried to build release builds but found out that on all projects I get the following two errors:

1. cannot find -lCMSISv1p30_LPC13xx    LPCXpresso1343_blinky        line 0    C/C++ Problem
2. make: *** [LPCXpresso1343_blinky.axf] Error 1    LPCXpresso1343_blinky        line 0    C/C++ Problem

Debug build works fine, which makes me wonder why the release build is having some issues.

As for the UART bug, it seems like when I try to run the V1.10 program for LPC1343 I get a computer freeze-up if I ran the debug and left it idle for 2 minutes. Hardware wise I used a PoUSB12 for connection to PC and software wise I used Docklight. It would be great if someone can shine some light on this issue. Thanks.
0 件の賞賛
返信
2 返答(返信)

858件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Techys on Sun Mar 07 03:15:04 MST 2010

Quote: CodeRedSupport
Hi,

You need to build the CMSIS project for Release too.



Hi. I found that project and built it too. Now things work fine. Thanks a lot.

Btw, I tried the release build but it did not solve the freezing problem. Even with a release build and not in debug mode, my computer will still freeze if I leave it idle with Docklight on. If a solution can be found that would be great. Thanks again.
0 件の賞賛
返信

858件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Mar 06 09:06:59 MST 2010
Hi,

You need to build the CMSIS project for Release too.
0 件の賞賛
返信