Question how to place a specific part of code in SPIFI and have the other part executed from SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question how to place a specific part of code in SPIFI and have the other part executed from SDRAM

595 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cojanprins on Tue Feb 17 07:11:20 MST 2015
Hello,

I'm working on a project with the integrated WEB server. I have already the project running, booting is from SPIFI, execution from SDRAM. Everything works OK. What I want to achieve is to keep the HTML code in SPIFI (not necessary to copy them at startup into SDRAM, thus saving RAM space).

All my HTML files (automatically converted into C "const unsigned char" arrays) are included in html_list.c, so result of the linkers shows it as: (actually a lot more files are present).


.rodata.ENG_homerepl
                0x00000000      0x6dc ./html/html_list.o
.rodata.ENG_trylogin
                0x00000000      0x2e0 ./html/html_list.o

Is there any way to inform the linker to have all .rodata. from html_list.o to remain with the address range of the SPIFI?

Thanks in advance.

Cojan Prins (The Netherlands)
0 项奖励
回复
4 回复数

584 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cojanprins on Tue Feb 24 00:30:59 MST 2015
OK, thank you for your reply, that's exactly the info I was looking for  :)
0 项奖励
回复

584 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 19 06:36:21 MST 2015
You are going to need to modify the linker script in a similar way to in this post...
http://www.lpcware.com/content/forum/running-cmsis-dsp-library-function-ram#comment-1138707

Regards,
LPCXpresso Support
0 项奖励
回复

584 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cojanprins on Tue Feb 17 08:29:07 MST 2015
For now I have done it by adding folowing lines to the link-file. This works. But now I have all constants in SPIFI flash and all executable code (text) in SDRAM.

I would like to have it more specific, to have all rodata from a specific object file in a certain location in the SPIFI. The option mentioned in the article above describes how to do it for each individual procedure or declaration. I would like to do it for all procedures/declarations from ONE object file. Is that possible?

    /* All constant tables, HTML pages etcetera can remain within SPIFI flash to reduce SDRAM usage */
    .constant_data : ALIGN(4)   
    {
        *(.rodata .rodata.* .constdata .constdata.*)
        . = ALIGN(4);
    } >Flash_00

    /* Executable code should be copied from SPIFI flash into SDRAM for better performance          */
    .text : ALIGN(4)   
    {
         *(.text*)
        . = ALIGN(4);
    } >SDRAM_00 AT>Flash_00
0 项奖励
回复

584 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 17 07:34:09 MST 2015
Please read this FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/coderodata-different-flash-blocks
0 项奖励
回复