Project runs when I exit LPCxpresso (using LPC1769)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project runs when I exit LPCxpresso (using LPC1769)

444件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lucassvarela on Mon Sep 28 06:21:03 MST 2015
Hi everyone. I've been having an issue with LPCxpresso and my LPC 1769 (on Windows 7). The problem is that when I build a project and debug it my target seems to be turned off (No LEDs shining or blinking) and when I exit LPCxpresso, the project I debugged starts to work perfectly (I hear the sound of a USB device connected when I close the software). I tried by clicking on the Run button but it didn't work. "Step by step" option or "Step over" neither. I installed correctly this software (it's activated) and target's driver but I don't know what the root of this issue.  Also I reinstalled the expresso, changed
workspace's directoty, etc. The programme recognized well my target after i had installed its driver. I also tried all USB ports but the problem persists. It's a pity I can't see in which part of the main code the LPC is because of this.

Here some specs:

Soft version: LPCxpresso v7.9.0
Windows version: Windows 7 Home Premium 64 bits
Link of LPC driver I've installed: https://www.lpcware.com/content/nxpfile/lpcxpresso-link2-usb-driver-package

Thanks. Hope I can find a solution soon.
0 件の賞賛
返信
0 返答(返信)