Project Includes - Preprocessor Include Paths

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Project Includes - Preprocessor Include Paths

1,426 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Thu Jun 12 11:42:24 MST 2014
Win 7-64/LPCXpresso v7.2.0

(Project)/Includes

I had created a project with two incorrect include paths for the _board and _chip paths. This causes a warning mark to
be displayed (project exclamation point inside triangle icon), indicating that something is amiss, even after a correction.

Looking at the (Project)/Includes I see the two files that are greyed out as not resolved.

Checking the project Preprocessor Include Paths, Macros etc., I see that the Debug build has two entries in CDT Managed Setting Entries, both of which describe the two non-existent files. However, the Action area (Add, Edit, Clear, Export) is also greyed out.

How can this be resolved short of a Delete/re-build of this Debug configuration?
0 项奖励
回复
4 回复数

1,405 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Mon Jun 16 16:51:42 MST 2014
Sorry, but I did not see the notification for your response, and at the moment it seems I deleted & re-created that project since I couldn't clean.

I will try to re-create, but this may have been caused by cut/paste with different projects. That practice has been found to create more problems that it's worth.

0 项奖励
回复

1,405 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jun 13 01:30:43 MST 2014
Yes, this did change in v7.2. However, a rebuild should clear the settings. Indeed, on the examples I have tried, these paths are reset. As I am unable to reproduce the problem, can you provide an example so that we can investigate?
0 项奖励
回复

1,405 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capstone on Thu Jun 12 16:20:25 MST 2014
Thanks, but my belief is that the Discovery Options are a v6.x setting and is not available in the v7.2

I realize that the build is ok, it's just un-clean.

In v7 it seems to be Preprocessor Include Paths - I see them there, but can't get them to be active.


0 项奖励
回复

1,405 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Jun 12 13:23:32 MST 2014
http://www.lpcware.com/content/faq/lpcxpresso/invalid-project-path-warnings
0 项奖励
回复