Programming issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming issues

1,035件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jx1 on Wed Jun 12 01:28:39 MST 2013
Hi,

From the code, it shows that the value of busy_led_state is toggle each time when dali_cmd is true. get_dali_cmd will get a message from DALI ballast or else will not return. I am trying to find out if the get_dali_cmd() gets stuck so I want to use the LED D4(dali master lpc1343) within get_dali_cmd. As LED D4 is not used in the program so I am using it for debugging purpose. Anyone has similar programs that can guide me?

Also please refer to the image
Thanks
0 件の賞賛
返信
0 返答(返信)