Program is not leaving the ISR (timer0 mat0 interrupt)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program is not leaving the ISR (timer0 mat0 interrupt)

936件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emielzij on Wed Dec 17 09:03:21 MST 2014
I have an external clock source that drives the counter0 of the LPC11C24.
If the counter value matches the match register 0 (in the code forced to a value 10 for testing purposes) then the counter should reset to 0 and the code should jump to an isr.

Here is my code:

#define timer0match 10//0-65535

#include "LPC11xx.h"

void timer0init(void)
{
LPC_IOCON->PIO0_2 |= (1 << 1);//Selects function CT16B0_CAP0
LPC_SYSCON->SYSAHBCLKCTRL |= (1 << 7);//Enable clock for 16-bit counter/timer0
LPC_TMR16B0->CTCR |= (1 << 0);//TC incremented on rising edge CAP input (Selected)

//CAP0 as clock source, default CAP0

//Configure CT16B0_MAT0 (PIO0_8) as match function for external measurements
LPC_GPIO0->DIR |= (1 << 8);        //Set PIO0_8 as output
LPC_TMR16B0->EMR|= 0x00000030;//EMC0, Toggle the corresponding External Match bit/output
LPC_IOCON->PIO0_8|= (1 << 1);        //Selects function CT16B0_MAT0

LPC_TMR16B0->MR0 = timer0match;//Set match value
LPC_TMR16B0->MCR|= (1 << 0);        //Interrupt if TC==MR0
LPC_TMR16B0->MCR|= (1 << 1);       //Reset TC to 0 if TC==MR0

LPC_TMR16B0->TCR |= (1 << 0);//Enable timer 0

//Reset timer 0
LPC_TMR16B0->TCR |= (1 << 1);
LPC_TMR16B0->TCR &= ~(1 << 1);

NVIC_EnableIRQ(TIMER_16_0_IRQn);
}

int main(void)
{
int i=0;

    LPC_SYSCON->SYSAHBCLKCTRL   |= (1<<6);//GPIO CLOCK ENABLE
    LPC_SYSCON->SYSAHBCLKCTRL   |= (1<<16);//Enable IOCON

    LPC_GPIO0->DIR|= (1 << 3);//OUTPUT
    LPC_IOCON->PIO0_3&= ~(1 << 3);        //Disable pull up

    timer0init();

    while(1)
    {
    LPC_GPIO0->DATA|= (1 << 3);
    for(i=0; i<100; i++);
    LPC_GPIO0->DATA &= ~(1 << 3); //toggle pin
    for(i=0; i<100; i++);

    }
    return 0 ;
}

void TIMER_16_0_IRQHandler(void)
{
LPC_TMR16B0->IR |= (1 << 0);//Clear interrupt flag by writing a 1
}


The PIO0_3 is not toggled in the while(1) loop, the program get stuck in the ISR I think. If I remove NVIC_EnableIRQ(TIMER_16_0_IRQn); from the code, the program runs fine. The hardware interrupt, toggle a pin at a match works fine in both cases.

Am I doing something wrong with the interrupt clearing?
0 件の賞賛
返信
2 返答(返信)

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emielzij on Wed Dec 17 14:38:45 MST 2014
Indeed, the ISR name was incorrect.
Thank you
0 件の賞賛
返信

902件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Dec 17 10:18:10 MST 2014

Quote: emielzij
...the program get stuck in the ISR I think.



:quest:

And what's the debugger telling you?

Probably your ISR name is wrong :((

void TIMER[color=#f00]_[/color]16_0_IRQHandler(void)

0 件の賞賛
返信