Program in flash cannot run again

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program in flash cannot run again

1,075 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maobiao.yao on Tue Oct 22 01:16:47 MST 2013
I have two projects. One is the sample LPCX1227_cmsis2_systick. I compile it and debug it. It runs very well.
I power off the device(disconnect it from PC) and power on it. the program in flash can run again.

the other project which is from the NXP(RC663-LPC1227-Polling), I can debug it too.
But when I repeat the steps described above(power off, then power on), It can not run again.

I don't know why.
I use the same board and same IDE.  LPCXpresso V6.0.4 Build 159  2013-10-09
Ubuntu 12.04
0 Kudos
Reply
3 Replies

1,059 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Oct 22 19:41:26 MST 2013
For mor information on Semihosting, see this FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/semihosting

And for more information on how to change the library type ,see:
http://www.lpcware.com/content/faq/lpcxpresso/library-variants
0 Kudos
Reply

1,059 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by maobiao.yao on Tue Oct 22 19:21:04 MST 2013
Thanks for your reply. Do you mean that if you use the feature of semi-hosting, your program only run in debug state?
When a project has the feature of semi-hosting, how to disable it?

0 Kudos
Reply

1,059 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Oct 22 07:16:58 MST 2013
No idea what "RC663-LPC1227-Polling" might be, but the first thing to check would be whether it uses semihosting:

http://www.lpcware.com/content/faq/lpcxpresso/semihosting

Regards,
LPCXpresso Support
0 Kudos
Reply