Production Programming via SWD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Production Programming via SWD

1,032件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuelpowell on Tue Jun 22 16:35:31 MST 2010
Hi,

Are there any problems with production programming an LPC1114 target using the LPC-link SWD and a release build in the eclipse IDE?

Since I want to expose the SWD header on the PCB, I'd rather not have to bring out the ISP pins as well, if this can be avoided.

Regards,

Sam.
0 件の賞賛
返信
2 返答(返信)

981件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuelpowell on Wed Jun 23 05:41:59 MST 2010
Thank you.

Regards,

Sam.
0 件の賞賛
返信

981件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 23:47:16 MST 2010
Yes, this will work.

You can use the command line flash programmer to program your device, so you don't need load the IDE. Use of the command line flash programmer is described in the Knowledgebase article:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/51
0 件の賞賛
返信