Production Programming via SWD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Production Programming via SWD

1,060 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuelpowell on Tue Jun 22 16:35:31 MST 2010
Hi,

Are there any problems with production programming an LPC1114 target using the LPC-link SWD and a release build in the eclipse IDE?

Since I want to expose the SWD header on the PCB, I'd rather not have to bring out the ISP pins as well, if this can be avoided.

Regards,

Sam.
0 项奖励
回复
2 回复数

1,009 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuelpowell on Wed Jun 23 05:41:59 MST 2010
Thank you.

Regards,

Sam.
0 项奖励
回复

1,009 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 23:47:16 MST 2010
Yes, this will work.

You can use the command line flash programmer to program your device, so you don't need load the IDE. Use of the command line flash programmer is described in the Knowledgebase article:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/51
0 项奖励
回复