Production Programming via SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Production Programming via SWD

1,027 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuelpowell on Tue Jun 22 16:35:31 MST 2010
Hi,

Are there any problems with production programming an LPC1114 target using the LPC-link SWD and a release build in the eclipse IDE?

Since I want to expose the SWD header on the PCB, I'd rather not have to bring out the ISP pins as well, if this can be avoided.

Regards,

Sam.
0 Kudos
Reply
2 Replies

976 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuelpowell on Wed Jun 23 05:41:59 MST 2010
Thank you.

Regards,

Sam.
0 Kudos
Reply

976 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 23:47:16 MST 2010
Yes, this will work.

You can use the command line flash programmer to program your device, so you don't need load the IDE. Use of the command line flash programmer is described in the Knowledgebase article:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/51
0 Kudos
Reply