Problems with Library Inclusions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with Library Inclusions

1,663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DreamM0d3 on Thu Jan 30 04:33:02 MST 2014
Hi,

I am using an LPC1769 board and running the latest version of LPCXpresso on my MBP.
I have an issue where I keep getting unresolved inclusion errors or no such file or directory when I compile my main.c
I do not get errors for includes such as "stdio.h" and "string.h", however I am unable to include other library files (etc "lpc17xx_pinsel.h")
I have all the library files in my workspace. I have tried using project reference, manual library linking and manual includes but to no avail. Would appreciate some advice on what could be the problem.


0 Kudos
Reply
4 Replies

1,544 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DreamM0d3 on Thu Jan 30 06:15:26 MST 2014
Hmm I imported my program and libraries onto another MBP and installed Xpresso on it too. So far everything runs perfectly fine. I suspect it could be a much deeper problem. Thanks for the prompt response anyway!
0 Kudos
Reply

1,544 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jan 30 06:05:22 MST 2014
Presumably you didn't follow the instructions correctly, because the FAQ explains exactly what you need to do.

p.s. Your picture does not display.
0 Kudos
Reply

1,544 Views
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by DreamM0d3 on Thu Jan 30 05:47:39 MST 2014
I did refer to that FAQ before posting here. This is the screenshot for your reference. Anyone else can help me out with this cause its rather urgent.

0 Kudos
Reply

1,544 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jan 30 05:02:45 MST 2014
Please read this FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/creating-linking-library-projects
0 Kudos
Reply