Problems when flashing NGX LPC4330-Xplorer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems when flashing NGX LPC4330-Xplorer

698件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Reinhard Huck on Thu Feb 04 08:43:33 MST 2016
Hi,

I try to flash an application to the NGX LPC4330-Xplorer board using LPCXpresso v8.0.0 [Build 526] [2015-11-23] on Windows 10 64 Bit. During the flash process I get the following error:

Error in final launch sequence
Failed to execute MI command:
-target-download
Error message from debugger back end:
Could not write registers; remote failure reply 'E22'
Could not write registers; remote failure reply 'E22'


So my question is: How to flash the NGX LPC4330-Xplorer board using LPCXpresso v8.0.0 (is there something to be considered)?

Thanks in advance,
Reinhard
0 件の賞賛
返信
1 返信

642件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Feb 04 10:30:39 MST 2016
I presume you've connected an external debug probe? You didn't mention any details about the LPC-Link2 (or other) probe connection. Can you post the project debug log in your reply?

Thanks and regards,
LPCXpresso Support
0 件の賞賛
返信