Problems Connecting to VM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems Connecting to VM

725件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ewajs on Sun Jun 16 16:33:20 MST 2013
Hi,
I'm currently using a MacBook Pro running OS X (10.8.3) and I have a VM (via Parallels Desktop) running XP SP2 with LPCXpresso 5 on it, whenever I try to debug (on a non modified LPC1769 Kit) I get the same message:
"Premature end of file.:null(line:1, Col:1)"
And see that the VM is not detecting my board.
I'm working with another Windows based computers and had to install the VM because I wasn't able to import the Windows Projects on my LPCXpresso running on OS X (they were FreeRTOS projects).

Parallels Windows detects the board, but not the LPCXpresso on XP SP2. I could initially program the board in the Mac version of LPCXpresso but when I started using freeRTOS i couldn't import existing projects and make them work on the Mac version.

Thanks in advance.
0 件の賞賛
返信
1 返信

704件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jun 17 02:03:37 MST 2013
Exactly which version of LPCXpresso 5 are you using? 5.2.4 is the latest at present.

In my personal experience, the usual problem  when using VMs is that wrong OS has grabbed the link. And check the FAQs on using LPC-Link under VM's...

http://support.code-red-tech.com/CodeRedWiki/CodeRedFAQ#VirtualMachine

Regards,
CodeRedSupport
0 件の賞賛
返信