Problem with watchpoints.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with watchpoints.

923件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Mon Nov 14 18:38:27 MST 2011
I am working with a LPC1114/301 and LPCXpresso ver 4.1.0_190.
If I set a single watchpoint the watchpoint seems to work correctly.

If I set two watchpoints then the LPCXpresso hangs up.   It does not appear
to break.   The watchpoints would not have been hit during this test.

If I hit the "suspend" button to stop the processor I get a popup that
says "crt_emu_lpc11_13_nxp.exe has stopped working.   I can terminate
the debug session and restart it OK.

The manual says that the chip has 2 watchpoints.   Is there any
reason for my problem?

Thanks,
Pete.
0 件の賞賛
返信
2 返答(返信)

910件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micrio on Mon Nov 14 18:57:23 MST 2011
I am not using semihosting but I did change the setting from "auto" to "off".
There was no change in the problem.

Thanks,
Pete.
0 件の賞賛
返信

910件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Nov 14 18:44:08 MST 2011
Are we talking about semihosting projects?

http://support.code-red-tech.com/CodeRedWiki/DebuggerSemihosting?highlight=%28watchpoint%29
0 件の賞賛
返信