Problem with switching between power-down-mode and sleep-mode (LPC1769)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with switching between power-down-mode and sleep-mode (LPC1769)

690件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ledmaster on Fri Aug 10 02:44:19 MST 2012
Hello, in my application I'm switching between the two energy-safe-modes power-down and sleep.
I can only use sleep or  power-down, but if I want to use both of them, the switch from power-down to sleep will cause the controller to reset while writing "0x00" to PCON.

Does anybody have this problem too?

Yannick
0 件の賞賛
返信
1 返信

678件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CroesJeroen on Fri Aug 10 14:36:49 MST 2012
I thought you could only use one of the modes. Like sleep, deep sleep or deep power down. I think you can't use two at the same time, that's why 3 modes are defined ( I think so)
0 件の賞賛
返信