Problem with starting debug session

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with starting debug session

615 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by doru on Tue Mar 03 06:52:06 MST 2015
Hi,
After my hdd crash, i have reinstaii WinXP (home edition) and latest LPCXpresso IDE LPCXpresso v7.6.2 [Build 326].
For LPC812 MCU and blinky project, i have try to start a debug session.
This message appear:

No compatible emulators available.
They may be disconnected, not powered, already in use or not compatible with this target

I have try with 2 different LPCXpresso board, (one of this is new)

On first conection, windows have install this usb device with DFU capabilities (LPCXpresso).
What can be the problem?

Thank you for help.
Doru
0 Kudos
Reply
1 Reply

601 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Mar 03 07:06:00 MST 2015
Which board are you using?

If you are using an LPCXpresso-MAX board (http://www.lpcware.com/content/devboard/lpcxpresso-max-developer-boards) then you need to make sure that you have installed the mbed serial port driver.

If you are using an LPCXpresso V1 board (http://www.lpcware.com/LPCXpressoV1Boards), then I would suggest working through the troubleshooting section of http://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link

PS - you should note that as per the release notes, Windows XP is no longer a supported platform (though we aren't currently aware of any issues).

Regards,
LPCXpresso Support
0 Kudos
Reply