Problem with "Program Flash"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with "Program Flash"

9,626件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 00:45:17 MST 2014
Hi,
I am using LPC1769 and LPC Expresso_7.3.0_186
I am using 64 bit windows 7. I was able to run the program in the Debug mode. But it is not possible to use the "Program Flash" option.
I am getting an error like this:
"53: License does not permit flash operations from the command line"

I tried reactivation also. But still i am getting the same problem. Please give a solution to this problem.
0 件の賞賛
返信
17 返答(返信)

9,555件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Sep 17 05:26:44 MST 2014
Not much more we can do to help then. I suggest that you sit down and compare your setup with your colleagues in order to work out why their systems work and your's doesn't. Please report back if you identify the issue.

You really should try to sort out why you are getting the error about the DLL too. That should have been installed during the install process and we have never seen a case where this has not occurred.

Regards,
LPCXpresso Support
0 件の賞賛
返信

9,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Wed Sep 17 04:48:50 MST 2014
Hi,

I dont want to share IP configuration details.
The output i got when i typed "crt_emu_cm3_nxp -info-license" is attached
0 件の賞賛
返信

9,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Sep 17 02:51:43 MST 2014
Sorry, but this does not show anything obviously wrong, so lets try some more things:

1. Open a command window
2. type:
c:\nxp\LPCXpresso_7.3.0_186\lpcxpresso\bin\Scripts\LPCXpressoPath.cmd
3. type:
set
4. type:
ipconfig/all
5. type:
crt_emu_cm3_nxp -info-license

Please post ALL of the output from running these commands
0 件の賞賛
返信

9,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Wed Sep 17 01:34:23 MST 2014
I have attached the text file created
0 件の賞賛
返信

9,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Sep 17 00:18:51 MST 2014
So this would indicate an environmental issue with your computer.

Please open a DOS command prompt (Go to the start menu and enter 'cmd' into the "Search programs and files" box), then enter the following sequence of commands…

env > envinfo.txt
ipconfig >> envinfo.txt
cscript >> envinfo.txt


And post the envinfo.txt file created.

Regards,
LPCXpresso Support
0 件の賞賛
返信

9,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 22:41:06 MST 2014
Hi,
I tried re-installing LPC Xpresso from scratch. But problem not solved yet.

I am using GUI Flash Program tool. and i got the output like this after getting the error.

---------------------------------------------------------------------------------------------------------------------------
Ni: LPCXpresso Debug Driver v7.3 (Jul  2 2014 14:55:57 - crt_emu_cm3_nxp.exe build 10)
Pc: (  0) Reading remote configuration
Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: HID64HS12
Nc: SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: Loaded LPC175x_6x_512.cfx: LPC175x_6x (512K) Jul  1 2014 11:51:13  On-chip Flash Memory

Nc: NXP: LPC1769  Part ID: 0x00000000
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=true
Cr:f PCXpresso Free License - Download limit is 8K (UNREGISTERED)
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed
---------------------------------------------------------------------------------------------------------------------------------------------------

Target Board: LPC 1769
Debug probe: LPc Link1
Firmaware: CMSIS
OS: Windows 7, 64 bit.

The thing which concerns me is that, my  colleagues are able to flash the program successfully using similar setup. But only i am facing the problem.
0 件の賞賛
返信

9,554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 16 07:29:50 MST 2014
The missing DLL message you are seeing is somewhat concerning. Did the drivers not successfully install during your original LPCXpresso installation ? It might be a good idea to try uninstalling then installing again from scratch.

But that aside, please can you:

- Confirm the actual command you are using to try to program the flash?

- Confirm the full output generated when you run the command?

You should be able to copy and paste these into this thread as text whether you are invoking the flash program from the command line or the GUI flash program tool.

Please also confirm what target MCU you are trying to program, and which debug probe you are connecting with. If you are using LPC-Link2, please also confirm if you are using redlink firmware (preferred) or CMSIS-DAP.

Please also confirm what OS you are running on.

Regards,
LPCXpresso Support
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 06:55:51 MST 2014
I have attached the output screen shot
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 16 06:39:07 MST 2014
...and what was the output from running
crt_emu_cm3_nxp -info-license
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 06:34:57 MST 2014
This problem is critical. Pls provide the solution.
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 06:10:48 MST 2014
i am attaching the files here.
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 16 05:59:12 MST 2014
Where is the log?
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 05:50:36 MST 2014
Hi,

I followed the instructions given in the FAQ. There is no problem in script engine. It is working fine.
Still i am facing problem in using "Program Flash" option and getting the error like this:
"53: License does not permit flash operations from the command line"

So i have run the debug driver in the diagnostic mode as suggested in the FAQ and i am am attaching the licence info file and .log file here.
Please go through it and provide a solution to this issue.
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 16 02:24:00 MST 2014
The error being reported is nothing to do with the size of the image. Please READ the FAQ we provided (especially the Windows section) and follow the instructions.

However, please note that the size of the file on disk (as reported by dir) is NOT the size of the image in flash.

We have some information on how to find the amount of flash used by your application here:
http://support.code-red-tech.com/CodeRedWiki/FlashRamSize
(this is an old Code Red FAQ which we have not yet ported to LPCWare - the information is still valid, however).
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HCTEK on Tue Sep 16 02:12:04 MST 2014
Hello,

to reduce the size of .axf file you may need to optimize your code. In other hand, to increase the maximum limit you need to purchase a Pro edition account.

Best regards,
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shambhu_hegde on Tue Sep 16 02:06:15 MST 2014
Thank you for your reply.
I read the FAQ mentioned by you.
The size of .axf file generated is 315 KB. But the limit is 256 KB.

So how can i reduce the size of .axf file?
Or is it possible to increase the maximum limit.
0 件の賞賛
返信

9,553件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 16 00:52:00 MST 2014
Please read this FAQ, which describes a similar license problem.
http://www.lpcware.com/content/faq/lpcxpresso/flash-image-too-large
0 件の賞賛
返信