Problem with LPC1115

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with LPC1115

1,046 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Wed Jan 21 09:01:02 MST 2015
Hello,

I was working with my board LPCXpresso and it suddenly shows on the screen:

Error in final launch sequence
  Failed to execute MI command:
-target-select extended-remote | crt_emu_lpc11_13_nxp -msg-port=49490 -g -mi -2 -pLPC1115/303 -vendor=NXP -e0 -wire=hid -flash-driver=LPC11_12_13_64K_8K.cfx
Error message from debugger back end:
Remote communication error.  Target disconnected.: No error.
  Remote communication error.  Target disconnected.: No error.


02: Failed on connect
  02: Failed on connect
  Bad ACK returned from status - wire error.
  Emu(0): Connected. Was: None. DpID:     EDB6. Info: HID64HS12



0 Kudos
Reply
2 Replies

1,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brattchess on Thu Jan 22 08:54:24 MST 2015
Hello LabRat,

Thanks!! Solved.
0 Kudos
Reply

1,028 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Wed Jan 21 09:29:41 MST 2015
Close LPCXpresso, reconnect LPC-link(2) and your board and open LPCXpresso again...

If that doesn't help, switch to ISP:

http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
0 Kudos
Reply