Problem reprogramming flash after WDT enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem reprogramming flash after WDT enabled

996 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdebliek on Mon Jun 21 10:23:31 MST 2010
I am working with the LPC11xx, and was testing the release version of the build, which enables the WDT. However, now that the WDT is enabled in the code residing in flash, I cannot reconnect with the debugger (using LPC-link) in order to reprogram the flash. I get the following error:

Error launching Release\<application>.axf
03: Failed on chip setup: Et: Flash driver not ready

Is there any way I can regain access via the debugger now?
Thanks.
0 项奖励
回复
2 回复数

986 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yasla on Thu Oct 10 05:22:25 MST 2013
You can mass erase before programming too. Works for me.
0 项奖励
回复

986 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rkiryanov on Mon Jun 21 11:01:47 MST 2010
Start bootloader - tie ISP pin to GND and reboot MCU.
0 项奖励
回复