Problem in lpc17xx_i2c.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in lpc17xx_i2c.c

893 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mfc on Sun Dec 05 02:56:55 MST 2010
I discovered a problem in the subject source code today -- I cannot find where to report it, so I'm putting it here in the hope that it might save someone some time.   The problem it causes is that the i2c2 clock runs twice as fast as specified, which could make some devices unreliable.

Mike Cowlishaw

Details:

[FONT=Courier New]In lpc17xx_i2c.c the I2C_SetClock function has an error; in the case of I2Cx == LPC_I2C2, the line[/FONT]
[INDENT][FONT=Courier New]  temp = CLKPWR_GetPCLK (CLKPWR_PCLKSEL_I2C1) / target_clock;[/FONT]
[/INDENT][FONT=Courier New]should be:[/FONT]
[INDENT][FONT=Courier New]  temp = CLKPWR_GetPCLK (CLKPWR_PCLKSEL_I2C2) / target_clock;[/FONT]

[/INDENT]
0 项奖励
回复
2 回复数

881 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mfc on Mon Dec 06 12:36:14 MST 2010

Quote: NXP_USA
Hi Mike,

That is a good catch. This change will be rolled into an upcoming LPC17xx example package release.

-NXP



It is an easy fix :-).   Sounds good.  Where is the right place to get the current updates, release, etc?  It's hard to find (I have not found it yet!).  And, ideally, a way to be notified of new updates.

Thanks -- Mike
0 项奖励
回复

881 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Mon Dec 06 11:28:46 MST 2010
Hi Mike,

That is a good catch. This change will be rolled into an upcoming LPC17xx example package release.

-NXP
0 项奖励
回复