Problem for accessing the development board in debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem for accessing the development board in debug

754件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ltugroup on Thu Jan 17 04:08:49 MST 2013
Hello,

We are using a LPC11C24 in the development board LPC11C24 LPCXpresso board (found here)

We currently can't access the board, the error windows are the ones in the attachment (Error_window1 appears first). I tried several methods as indicated in the datasheet:
[LIST]
[*]connect GND and ISP (P0_1) while reseting to prevent the program from launching
[*]launch a Vector Catch debug
[/LIST]

We think that this problem comes from the board since we tried to launch the same program in the same conditions on another board and did not have any problem.
We previously used the Deep sleep mode on this board, but since now we always managed to get out of it.

Did somebody already face that kind of error and could help us?

Thank you
0 件の賞賛
返信
1 返信

746件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jan 17 08:34:21 MST 2013
Switching to ISP isn't working :confused:

Wiki: www.support.code-red-tech.com/CodeRedWiki/DebugAccessChip

Video: http://www.youtube.com/watch?v=chFv1EiZcYo
0 件の賞賛
返信