Problem for accessing the development board in debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem for accessing the development board in debug

748 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ltugroup on Thu Jan 17 04:08:49 MST 2013
Hello,

We are using a LPC11C24 in the development board LPC11C24 LPCXpresso board (found here)

We currently can't access the board, the error windows are the ones in the attachment (Error_window1 appears first). I tried several methods as indicated in the datasheet:
[LIST]
[*]connect GND and ISP (P0_1) while reseting to prevent the program from launching
[*]launch a Vector Catch debug
[/LIST]

We think that this problem comes from the board since we tried to launch the same program in the same conditions on another board and did not have any problem.
We previously used the Deep sleep mode on this board, but since now we always managed to get out of it.

Did somebody already face that kind of error and could help us?

Thank you
0 Kudos
Reply
1 Reply

740 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jan 17 08:34:21 MST 2013
Switching to ISP isn't working :confused:

Wiki: www.support.code-red-tech.com/CodeRedWiki/DebugAccessChip

Video: http://www.youtube.com/watch?v=chFv1EiZcYo
0 Kudos
Reply