Pll

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pll

464 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by straw_hat on Fri Sep 23 00:55:44 MST 2011
Hello

Can I ask if how can I switch back the main clock after I wakeup from  deep sleep mode. Before I go to deep sleep, I switch the clock to IRC  because it is stated in the manual. After wake up it should switch back  to PLL using system PLL Clock Out. Where should I write the code that  switch back to PLL? Is it necessary in the Wakeup_IRQHandler?? Because  I've try to put it there but still the one that clocks my system is the  IRC. I am using the LPC1343:confused::confused:. Thank you
0 Kudos
Reply
0 Replies