Pb for example USBMSDROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pb for example USBMSDROM

819件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vinceda on Mon Sep 19 03:23:57 MST 2011
hello,

I try to run the example for the LPC1343 USBMSDROM and this example displays a removable disk in explorer and when I open the folder there should be a "readme.txt" file but I do not get this result.

I plugged my USB cable as in the data sheet LPC1343, and I execute the procedure described in the data sheet AN10905 but I get to explore a removable disk window and asks me to format, but I do not have removable drive named "USB LPC134x" and the file "read me.txt".

I work in Windows 7 (32 bit) and with the LPCXpresso LPC1343 board.

Thank you for your help.

vinceda
0 件の賞賛
返信
1 返信

813件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CC58 on Mon Dec 03 15:53:23 MST 2012
I get the same thing.  I see a drive, but no readme.txt file.
Also its asking me to format the drive.
Anybody have a fix?
0 件の賞賛
返信