PCB Layout Drawing for LPCxpresso LPC1769 Rev B ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCB Layout Drawing for LPCxpresso LPC1769 Rev B ?

811件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrews on Tue Oct 29 09:03:35 MST 2013
Is there a PCB layout drawing available for the LPCxpresso LPC1769 Rev B board?  It doesn't appear all the pins that are supposed to be connected to the expansion connector are connected based on the schematic I have.  For example, P0.22 does not go to the expansion connector on my board.  I could have a problem with my board but want to make sure the board is really laid out as shown in the schematic. 

Thanks
0 件の賞賛
返信
1 返信

720件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrews on Tue Oct 29 10:01:10 MST 2013
Disregard, I found the problem.  I misinterpreted the PIN numbers on the board.
0 件の賞賛
返信