PCB Layout Drawing for LPCxpresso LPC1769 Rev B ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PCB Layout Drawing for LPCxpresso LPC1769 Rev B ?

809 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrews on Tue Oct 29 09:03:35 MST 2013
Is there a PCB layout drawing available for the LPCxpresso LPC1769 Rev B board?  It doesn't appear all the pins that are supposed to be connected to the expansion connector are connected based on the schematic I have.  For example, P0.22 does not go to the expansion connector on my board.  I could have a problem with my board but want to make sure the board is really laid out as shown in the schematic. 

Thanks
0 项奖励
回复
1 回复

718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrews on Tue Oct 29 10:01:10 MST 2013
Disregard, I found the problem.  I misinterpreted the PIN numbers on the board.
0 项奖励
回复