Not able to program flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to program flash

4,028 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Mon Jun 21 09:06:00 MST 2010
After I connect the Xpresso board to the PC and after the LPC-Link gets initialized , if I try to program flash I get the following error -

LPCXpresso Error :

53 : Liscence does not permit flash operations from command line.

The program Im trying to flash is blinky.

Please help.

My computer is a netbook , 1.6GHz Intel atom , 2GB Ram hosts Windows Xp Professional SP 2.

Original Attachment has been moved to: 1100474_44_1KHz.txt.zip

0 项奖励
回复
15 回复数

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jun 23 07:03:42 MST 2010
Reinstalling the same product over and over again will make absolutely no difference. There was a problem in the code that affects a very very small number of computers, and this has been fixed in the new release. The new release will be made available when we have finished testing it.

The configuration of the other computers that experienced this problem is completely irrelevant.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Wed Jun 23 06:40:43 MST 2010
I have uninstalled and re-installed 3 times already , I have even created new E-mail Id's just for getting the Activation Key , but all effort is in vain.

When is the exact date the new release will be out ?

What is the config of the other 2 comps (OS specifically) ?
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Jun 23 05:16:48 MST 2010
Uninstall and then Re-install the new release. As it looks like there is a problem with the license, you may need to get a new serial number/activation code as well.

Note this this problem only affects a very small number of computers - yours is only the 3rd to have been reported.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Wed Jun 23 01:30:08 MST 2010
But the same release works in my Desktop (different Liscence No).
When installing this IDE in my desktop , when I clicked on the 3.3.4 Link it showed a window with Run, Save and cancel . I clicked on Run.

In my netbook , only Save File and Cancel appeared in the window even though both systems have Windows XP Prof SP 2.

So , I should uninstall and Re-install or upgrade the IDE when the new version is released ?
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 23:37:50 MST 2010
It looks like your license is not recognised by the Debug Driver. There will be a new release later this week that should resolve this issue.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Tue Jun 22 23:23:47 MST 2010
I tried the command with the modification you mentioned , ouput in cmd prompt is :

C:\nxp\lpcxpresso_3.3\bin>crt_emu_lpc11_13_nxp -g -4 -wire=winusb -pLPC1343 -fla
sh-load-partial=your_application.axf
Pc: ( 0) Reading remote configuration
Ni: LPCXpresso Debug Driver v2.0 (Apr 8 2010 14:57:58)
Nc: Looked for chip XML file in C:/nxp/lpcxpresso_3.3/bin/LPC1343.xml

Nc: Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.3/bin/nxp_direct
ory.xml

Nc: Found generic directory XML file in C:/nxp/lpcxpresso_3.3/bin/crt_directory.
xml

Pc: ( 5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: NXP: LPC1343 Part ID: 0444102B
Pc: ( 65) Chip Setup Complete
'ipconfig.exe' is not recognized as an internal or external command,
operable program or batch file.
'cscript.exe' is not recognized as an internal or external command,
operable program or batch file.
Wt: License check failure (CheckLicense)
Nt: Connected: was_reset=false. was_stopped=true
Cr:f Restricted - unregistered license, download limit of 8K
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed

When I go to Help-->Product Activation--> Display License type I get:

License Type : Full
Debug Limit : 128kb
Activation Code : B3BT-JVCT-LSFT-N3NZ-PXDV-D5CZ-BYDS-JXK5

A full copy of LPCXpresso may be used for production

Im using LPCXpresso 1114 , but in the output of command prompt its coming LPC1343 , I even went to Windows-->Preferences-->MCU settings and chose LPC1114/301.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Tue Jun 22 23:11:02 MST 2010
I tried the command with the modification you mentioned , ouput in  cmd prompt is :

C:\nxp\lpcxpresso_3.3\bin>crt_emu_lpc11_13_nxp -g -4 -wire=winusb  -pLPC1343 -fla
sh-load-partial=your_application.axf
Pc: (  0) Reading remote configuration
Ni: LPCXpresso Debug Driver v2.0 (Apr  8 2010 14:57:58)
Nc: Looked for chip XML file in C:/nxp/lpcxpresso_3.3/bin/LPC1343.xml

Nc: Looked for vendor directory XML file in  C:/nxp/lpcxpresso_3.3/bin/nxp_direct
ory.xml

Nc: Found generic directory XML file in  C:/nxp/lpcxpresso_3.3/bin/crt_directory.
xml

Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: NXP: LPC1343  Part ID: 0444102B
Pc: ( 65) Chip Setup Complete
'ipconfig.exe' is not recognized as an internal or external command,
operable program or batch file.
'cscript.exe' is not recognized as an internal or external command,
operable program or batch file.
Wt: License check failure (CheckLicense)
Nt: Connected: was_reset=false. was_stopped=true
Cr:f Restricted - unregistered license, download limit of 8K
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed

When I go to Help-->Product Activation--> Display License type I  get:

License Type : Full
Debug Limit  : 128kb
Activation Code : B3BT-JVCT-LSFT-N3NZ-PXDV-D5CZ-BYDS-JXK5

A full copy of LPCXpresso may be used for production
                 [IMG]http://knowledgebase.nxp.com/images/misc/progress.gif[/IMG] [IMG]http://knowledgebase.nxp.com/images/buttons/edit.gif[/IMG]

Im using LPCXpresso 1114 , but in the output of command prompt its coming LPC1343 , I even went to Windows-->Preferences-->MCU settings and chose LPC1114/301.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Tue Jun 22 23:07:35 MST 2010
I tried the command with the modification you mentioned , ouput in cmd prompt is :

C:\nxp\lpcxpresso_3.3\bin>crt_emu_lpc11_13_nxp -g -4 -wire=winusb -pLPC1343 -fla
sh-load-partial=your_application.axf
Pc: (  0) Reading remote configuration
Ni: LPCXpresso Debug Driver v2.0 (Apr  8 2010 14:57:58)
Nc: Looked for chip XML file in C:/nxp/lpcxpresso_3.3/bin/LPC1343.xml

Nc: Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.3/bin/nxp_direct
ory.xml

Nc: Found generic directory XML file in C:/nxp/lpcxpresso_3.3/bin/crt_directory.
xml

Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: NXP: LPC1343  Part ID: 0444102B
Pc: ( 65) Chip Setup Complete
'ipconfig.exe' is not recognized as an internal or external command,
operable program or batch file.
'cscript.exe' is not recognized as an internal or external command,
operable program or batch file.
Wt: License check failure (CheckLicense)
Nt: Connected: was_reset=false. was_stopped=true
Cr:f Restricted - unregistered license, download limit of 8K
Pc: ( 70) License Check Complete
Et:53: License does not permit flash operations from command line
Pc: (100) Target Connection Failed

When I go to Help-->Product Activation--> Display License type I get:

License Type : Full
Debug Limit  : 128kb
Activation Code : B3BT-JVCT-LSFT-N3NZ-PXDV-D5CZ-BYDS-JXK5

A full copy of LPCXpresso may be used for production
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 15:16:57 MST 2010
Try using -wire=winusb instead of -wire=hid

note that you must boot the lpcxpresso board first
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Tue Jun 22 09:43:04 MST 2010
I connected the board to my netbook and debugged blinky program just to initialize the LPC-Link , it debugged successfully.

From command line when I ran first bootLPCXpresso winusb it gave 'No device connected , press download when connected'.
When I ran the command you gave me I got the following output-

C:\nxp\lpcxpresso_3.3\bin>crt_emu_lpc11_13_nxp -g -4 -wire=hid -pLPC1343 -flash-
load-partial=your_application.axf
Pc: (  0) Reading remote configuration
Ni: LPCXpresso Debug Driver v2.0 (Apr  8 2010 14:57:58)
Nc: Looked for chip XML file in C:/nxp/lpcxpresso_3.3/bin/LPC1343.xml

Nc: Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.3/bin/nxp_direct
ory.xml

Nc: Found generic directory XML file in C:/nxp/lpcxpresso_3.3/bin/crt_directory.
xml

Pc: (  5) Remote configuration complete
Ed:02: Failed on connect: Ee(05). No matching emulator found - make sure power i
s on and not in use already.
Et:31: No connection to emulator device
Pc: (100) Target Connection Failed
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 08:48:10 MST 2010
That will boot LPCXpresso, if it needs it.

Could your now run the command that was in my earlier post.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Tue Jun 22 08:36:15 MST 2010
In the bin/Scripts folder these files are available -
bootLPCXpresso.cmd , finddfu.cmd , finddfu.vbs , findhid.cmd and findhid.vbs

I clicked on bootLPCXpresso.cmd but nothing happens other than the command prompt coming and closing after a sec or so.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jun 22 01:11:43 MST 2010
Hi,

Can you try running the flash programmer from the command line and list ALL of the output from the command

crt_emu_lpc11_13_nxp -g -4 -wire=hid -pLPC1343 -flash-load-partial=your_application.axf


Full details can be found here:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/51
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjvadithya1989 on Mon Jun 21 22:36:49 MST 2010
The version is 3.3.4.
Liscence type : Full
Debug Limit : 128kb

I am trying to program flash using the Program Flash Icon in the toolbar.
But, I am able to debug blinky successfully.
0 项奖励
回复

3,887 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Jun 21 09:52:17 MST 2010
Please can you confirm:


[LIST=1]
[*] What version of LPCXPresso you are using? The current release version is 3.3.4. Use "Help -> About LPCXPresso" to identify your current version.
[*] How are you trying to programme the flash? Using the "Debug" option in the Quickstart panel?
[*] Can you confirm the contents of the MCU Debug log when you try to debug?
[/LIST]
For example when I debug blinky I see:
 
LPCXpresso Debug Driver v2.0 (Apr  8 2010 14:57:58)
Looked for chip XML file in C:/nxp/lpcxpresso_3.3.4_169/bin/LPC1114/301.xml
Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.3.4_169/bin/nxp_directory.xml
Found generic directory XML file in C:/nxp/lpcxpresso_3.3.4_169/bin/crt_directory.xml
NXP: LPC1114/301  Part ID: 0444102B
Connected: was_reset=false. was_stopped=true
v Registered license, download limit of 128K
Writing 7488 bytes to 0000 in Flash (assumed clock: 48.0MHz)
Verified-same page 0-1 with 7488 bytes in 780msec
Flash write Done
nSRST assert (if available)
Executing in user flash.
Stopped
GDB trying to set entry point of 0x016D, but correct entry is 0x1FFF0040
nSRST assert (if available)
Executing in user flash.
Stopped: Breakpoint #1
To view the contents of the MCU debug log, select the "Console" view (typically middle of screen, towards the bottom), then select "MCU Debug log" from the drop down "terminal/PC" icon on the right hand side of the view.

Regards,
CodeRedSupport.
0 项奖励
回复