No Emulator Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No Emulator Error

633件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by calvin02168 on Tue Jun 19 23:07:54 MST 2012
hi all,

i have a LPCXpresso 1114/301 board, whereby when i connect it to my pc, the window install the driver for the board, than i downloaded the examples from NXP website and build it scuessfully, than when i click on debug, i get a no emulator error. i research on the internet and did the Diagnostic that is being suggested in this forum but i get the error of no divice connected. i check the connected usb at device manager and it state that the device is connected to windows, please advice
0 件の賞賛
返信
1 返信

625件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Tue Jun 19 23:29:17 MST 2012
Please do a search on this forum for "no emulator". I got 126 hits concerning this topic.
Most plausible causes are:
[LIST]
[*]bad usb cable or poor quality.
[*]usb port at the computer side doesn't deliver 500mA of current
[*]read this http://support.code-red-tech.com/CodeRedWiki/USBProblems
[*]and read this http://support.code-red-tech.com/CodeRedWiki/FailedToConnect
[/LIST]I hope this was helpful information.

Regards,
Serge
0 件の賞賛
返信