Need_Support...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need_Support...

696件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by murugeshp on Fri Mar 15 05:16:49 MST 2013
Hi,
      We have to develop  biocrypt application with LPC4337JET100 controller and we having OM13027 evaluation board and we looking on LPC link debugger and supported IDE and RTOS.
So could you please support & send to us required hardware and software components and those are free version or license version and where to purchase those components.

I hope, you understand that!...
0 件の賞賛
返信
1 返信

676件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Fri Mar 15 07:17:49 MST 2013
Did you try reading the 'readme.txt' file inside the project itself ? :rolleyes:


Quote:
If required, the webpage contents can be modified. To do this, change
the appropriate files in the \apps\webserver\httpd-fs subdirectory of
the project. You will then need to process these files into the data
files that get built into the executable. To do this, run the PERL
program "makefsdata" \apps\webserver.



HTH :D
0 件の賞賛
返信