Need LPC 1769 original bootloader file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need LPC 1769 original bootloader file

636 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ken_a on Fri Jun 22 17:25:45 MST 2012
Hello,
Does someone have a link, or info as to where I can get the boot-loader file such as the one the LCP1769 Xpresso board ships with.  I need to re-flash my board.

Many Thanks,
Ken Austin
0 项奖励
回复
1 回复

610 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jun 23 00:57:55 MST 2012
The bootloader is built into ROM and so cannot be changed or reprogrammed. Perhaps you just need to boot into ISP mode?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip
0 项奖励
回复