NMI Interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NMI Interrupts

711件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Jan 19 05:49:03 MST 2013
[FONT=Tahoma][SIZE=2]If I never configure the pin (Port 2 pin 10 on an LPC1778) [/SIZE][/FONT][FONT=Tahoma][SIZE=1][SIZE=2]for NMI, is it true that an NMI interrupt can [I]never[/I] happen?

Mike[/SIZE]
[/SIZE][/FONT]
0 件の賞賛
返信
1 返信

686件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by karanmehta93 on Sat Jan 19 14:17:49 MST 2013
Yes, The pin has multiple functions also. If not configured as input and NMI, by defaut it will work as a normal GPIO pin. And yes, Don't forget to put up external pull up on this pin.
0 件の賞賛
返信