NFC Reader Library | Blueboard PNEV512B|LPC1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC Reader Library | Blueboard PNEV512B|LPC1769

794 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sachinblitzkrieg on Tue Oct 14 23:23:10 MST 2014
Hi ,

I am trying to flash example project provided for LPC 1769, Which has all the NFC reader library and other necessary stuffs.
I have succesfully Interfaced Blueboard with LPC1769 and build the project  named Classic.

Am able to run the program in debug mode. But when i flash the classic.axf file to the board , Program is not running from the flash.

Need support immediately.
0 项奖励
回复
1 回复

664 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Oct 15 01:00:00 MST 2014
The normal reason for applications that run under the debugger failing when executing without flash connected is semihosting:

http://www.lpcware.com/content/faq/lpcxpresso/semihosting

But that aside, please ensure that if you are using the latest version of the examples for the Blueboard and have read the associated documentation. I know that the NFC division of NXP issued at an update a few months ago which should work correctly with the latest LPCXpresso v7 releases.

http://www.nxp.com/demoboard/CLEV663B.html#documentation

I don't have access to an appropriate board, so can't test here in any sensible manner - but if still see issues with the latest examples we can follow up with the NFC division, else you can contact them via the email link on the left hand side of:

http://www.nxp.com/demoboard/CLEV663B.html#support

Regards,
LPCXpresso Support

0 项奖励
回复