Modbus TCPIP Development Using LPC1769:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Modbus TCPIP Development Using LPC1769:

1,537 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hareesha on Mon Jan 30 22:32:53 MST 2012
[FONT=Times New Roman, serif][SIZE=3]Dear Friends,[/SIZE][/FONT]

[FONT=Times New Roman, serif][SIZE=3]In our application we are planning to use Modbus TCPIP communication. This communication is between [/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3][B]HMI[/B][/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3] and [/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3][B]LPC1769[/B][/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3] Microcontroller. I am having idea about TCPIP in TRANSPORT layer but this Modbus TCPIP is communicating in APPLICATION layer.[/SIZE][/FONT]
[FONT=Times New Roman, serif][SIZE=3]So is there any example code for [/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3][B]Modbus TCPIP??? [/B][/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3]If there plz can you give me.[/SIZE][/FONT]
[FONT=Times New Roman, serif][SIZE=3]If you have any useful data and links about [/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3][B]Modbus TCPIP,[/B][/SIZE][/FONT][FONT=Times New Roman, serif][SIZE=3] Plz give me.[/SIZE][/FONT]


[FONT=Times New Roman, serif][SIZE=3]Thanks & Regards,[/SIZE][/FONT]
[FONT=Times New Roman, serif][SIZE=3]Hareesha[/SIZE][/FONT]
0 Kudos
Reply
2 Replies

1,374 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hareesha on Tue Jan 31 21:22:44 MST 2012
Dear Sir,



Thanks for your replay,



I hope it will be useful. Is this code is general for any controller or specific to any particular controller???



Is there any other general Ethernet sample code for LPC1769.Because first I want test Ethernet link and communication between PC and LPC1769 board.


Thanks & Regards,
Hareesha
0 Kudos
Reply

1,374 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jan 31 03:47:06 MST 2012
There's a mbed sample:

http://mbed.org/users/tmav123/programs/ModbusTCP/m1pxgl
0 Kudos
Reply