Missing registers in Peripheral view

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing registers in Peripheral view

804件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nebarto on Thu Sep 27 19:51:03 MST 2012
I am trying to look certain registers on the LPC11U37 USART (which shows up as a UART in the debug peripheral list) The missing registers appear to be SYNCCONTROL and SCICControl among others.

Is there any way to manually add these in myself or do I have to wait for Code red to fix this?
0 件の賞賛
返信
3 返答(返信)

795件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Sep 29 06:55:21 MST 2012

Quote: nebarto
I am trying to look certain registers on the LPC11U37 USART (which shows up as a UART in the debug peripheral list) The missing registers appear to be SYNCCONTROL and SCICControl among others.


Thanks for highlighting this. I've logged the issue for investigation and fixing in a future release.

Regards,
CodeRedSupport
0 件の賞賛
返信

795件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Brutte on Fri Sep 28 12:25:37 MST 2012

Quote: MikeSimmonds
[SIZE=2][FONT=Tahoma](..)This means that you have to wait for Code Red to correct/add peripheral view details.(..)[/FONT][/SIZE]


or

Quote: Brutte
use EmbSysRegView

0 件の賞賛
返信

795件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Fri Sep 28 01:19:34 MST 2012
[SIZE=2][FONT=Tahoma]The peripheral view setup info for a particular processor is defined in an xml file [B]BUT[/B] ...
Code Red (it appears to me) deploy [I]encrypted[/I] xml.

This means that you have to wait for Code Red to correct/add peripheral view details.

It's a bummer, but you can understand them wanting to protect their intellectual property development efforts.
[/FONT][/SIZE]
0 件の賞賛
返信