Missing Product Activation Menu Option

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing Product Activation Menu Option

1,219件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by coco on Wed Jul 17 20:41:06 MST 2013
Hi guys,

I'm very new to LPC and just installed the LPCXpresso v5.2 in my Ubuntu machine (11.10 64 bit). The problem is I couldn't find that Help->Product Activation selection in my installation. I tried to uninstall and reinstall back older version of LPCXpresso (5.1 and 5.0) with no luck. That selection is still missing. Anyone encounter this before? Is there any temporary files that LPCXpresso created which I can try to clear? Thanks for the help.

coco
0 件の賞賛
返信
4 返答(返信)

1,210件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by coco on Sun Jul 21 18:57:14 MST 2013
Hi guys,

Just to update, I manage to find the culprit. It's not the unity interface. I was using the same workspace folder for LPCXpresso and Eclipse, and that is the cause of the problem. Creating a new workspace folder for LPCXpresso resolve the issue. I guess it got confused with .metadata created by the Eclipse.

0 件の賞賛
返信

1,210件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 18 00:57:45 MST 2013
I suspect that you need to apply the shell script workaround for the "Ubuntu Unity interface" detailed in...

http://support.code-red-tech.com/CodeRedWiki/RunningOnLinux

Regards,
LPCXpresso Support

0 件の賞賛
返信

1,210件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by coco on Thu Jul 18 00:33:38 MST 2013
Yes I run the LPCXpresso and open the Help. Here is the list of options shown in the Help:

Help Contents
Search
Dynamic Help
-----------------
Tips and Tricks ...
-----------------
Check For Updates
Install New Software
-----------------
About LPCXpresso


Thanks.
0 件の賞賛
返信

1,210件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Jul 17 23:24:01 MST 2013
Did you run LPCXpresso? These menu items are in the product - not on the desktop.

If this is not your problem, I suggest you take a snapshot of the LPCXpresso menu bar and post it to the forum.
0 件の賞賛
返信