Missing C++ Project Wizards in LPCXpresso for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing C++ Project Wizards in LPCXpresso for Linux

2,963件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Fri Oct 01 11:51:52 MST 2010
In 2nd beta of LPCXpresso for Linux there are no wizards for C++ projects.

Is something wrong in my installation or they will come in the release version?

Regards,
mrib
0 件の賞賛
返信
7 返答(返信)

2,940件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Oct 05 23:38:56 MST 2010
As I said:

Quote:

The [B]latest [/B]version of the Windows product offers the exact same options as the Linux product.

0 件の賞賛
返信

2,938件の閲覧回数
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by mrib on Tue Oct 05 15:07:52 MST 2010


Quote: CodeRedSupport
The latest version of the Windows product offers the exact same options as the Linux product.

As we have already stated, C++ development is not supported in LPCXpresso.


I attached 2 print screens showing that Windows version has C++ wizards and Linux version does not.

Under Windows I created a C++ project and could compile it (debugging not tried yet).

Maybe I missed something but they are not the same.

0 件の賞賛
返信

2,938件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Oct 05 08:06:45 MST 2010
The latest version of the Windows product offers the exact same options as the Linux product.

As we have already stated, C++ development is not supported in LPCXpresso.
0 件の賞賛
返信

2,938件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Tue Oct 05 07:35:54 MST 2010

Quote: CodeRedSupport
Sorry, LPCXpresso is C only. If you want to carry out C++ development then you will need to purchase one of the paid-for Red Suite variants. For more details, please see:

http://www.code-red-tech.com/products.php#comparison

Regards,
CodeRedSupport



I would like to come back to this topic:

Is there a reason why the windows version of LPCXpresso provides C++ wizards and the Linux version does not?

Does the C++ wizards come with the release version of Linux?

Thanks,
mrib
0 件の賞賛
返信

2,938件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mrib on Fri Oct 01 12:39:30 MST 2010

Quote: CodeRedSupport
Sorry, LPCXpresso is C only. If you want to carry out C++ development then you will need to purchase one of the paid-for Red Suite variants. For more details, please see:

http://www.code-red-tech.com/products.php#comparison

Regards,
CodeRedSupport



Thanks for the info.
But why are the C++ wizards in Windows version included?

Regards,
mrib
0 件の賞賛
返信

2,938件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Fri Oct 01 12:35:18 MST 2010
Hello,

I see an available option: File - New - Project... - C++ Project

I thought that C++ was not suitable for microcontrollers with little memory.

I do not like C, much less C++ :D
0 件の賞賛
返信

2,938件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Oct 01 12:03:40 MST 2010
Sorry, LPCXpresso is C only. If you want to carry out C++ development then you will need to purchase one of the paid-for Red Suite variants. For more details, please see:

http://www.code-red-tech.com/products.php#comparison

Regards,
CodeRedSupport
0 件の賞賛
返信