Make version included in LPXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Make version included in LPXpresso

500 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zarrro on Wed Dec 26 04:16:52 MST 2012
Hello :)

I just tried to import a library i have  with custom Makefiles in LPCXpresso, and I noticed something interesting. LPCXpresso is bundled with [B]ancient[/B] version of make. For portable code I use my own makefiles and since 3.81 is out as stable version for 6 years already I am happily using eval.
But it turns out that the make version in LPCXpresso is 3.79, was released [B]ONLY[/B] 12 year ago in 2000. While this is OK for projects generated by LPCXpresso , it is simply ridiculous for any non Xpresso generated project.

So I just wanted to say:

[SIZE=5]Please , in the next release , bundle a version of make which is more recent than the dinosaurs :)
[SIZE=5]
[SIZE=5][SIZE=3][SIZE=3][SIZE=3]Bye[SIZE=3], and thanks for the [SIZE=3] [/SIZE][/SIZE][/SIZE][/SIZE][/SIZE][/SIZE][SIZE=3]nice tools :)[/SIZE]
[/SIZE][/SIZE]
0 项奖励
回复
0 回复数