LPCXpresso Announcements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Announcements

2,091件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Mon Nov 30 15:47:00 MST 2009
[COLOR=black][SIZE=4][FONT=Arial]Hello,

The LPCXpresso forum is now active and ready for use! NXP extends a warm welcome to all LPCXpresso users. We will be actively supporting the LPCXpresso community on the forum.

Please visit the links below to get going with LPCXpresso:

LPCXpresso webpage:
[/FONT][/SIZE][SIZE=4][FONT=Arial]www.nxp.com/lpcxpresso[/FONT][/SIZE]
[/COLOR][COLOR=black][SIZE=4][FONT=Arial]
Download link for Getting Started Guide:
[/FONT][/SIZE][SIZE=4][FONT=Arial]www.standardics.nxp.com/support/lpcxpresso/pdf/getting.started.pdf[/FONT][/SIZE]
[/COLOR][COLOR=black][SIZE=4][FONT=Arial]
Application support page for LPCXpresso: (Examples and FAQs)
[/FONT][/SIZE][/COLOR][COLOR=black][SIZE=4][FONT=Arial]www.nxp.com/lpcxpresso-support
[/FONT][/SIZE][/COLOR]
0 件の賞賛
返信
8 返答(返信)

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Dec 15 08:57:47 MST 2010
The following new files have been released recently:

On www.code-red-tech.com/lpcxpresso:
LPCXpresso v3.6 for Windows
(linux update version to come soon)

On www.nxp.com/lpcxpresso-support:
FreeRTOS Demo and Docs for LPC13xx and LPC17xx (also posted on FreeRTOS's web site)
New Example Projects bundle for the LPC1xxx family.

Thank you,
-NXP
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Oct 06 11:25:16 MST 2010
The LPCXpresso for Linux Beta 2 is available!

LPCXpresso is now available for Linux- the installer can be downloaded from www.code-red-tech.com/lpcxpresso after creating a free account.

Please try it and provide feedback.

Thank you,
-NXP
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Jul 15 10:58:15 MST 2010
New LPCXpresso Examples Posted

Several new examples are available at http://www.nxp.com/lpcxpresso-support

They are:
     A FreeRTOS example for the LPC11xx
     Stack usage monitoring examples for the LPC11xx, LPC13xx, and LPC17xx
     New example projects for the LPC17xx & EA baseboard
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Tue May 11 12:01:46 MST 2010
LPCXpresso V3.3 was released in April, 2010.

Please visit www.code-red-tech.com/lpcxpresso to download the latest version.

Enhancements:
This release adds support for 64-bit Windows XP, Windows Vista, and Windows 7 platforms.
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Feb 24 03:18:10 MST 2010
Embedded Artists offers many LPCXpresso-focused products that can also be used with mbed.

Overview
--------
LPCXpresso Base Board- a feature-rich expansion board
http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php

LPCXpresso Proto Board- large prototyping board with through-hole and surface mount pads
http://www.embeddedartists.com/products/lpcxpresso/xpr_prototype.php

LPCXpresso Value Pack- LPCXpresso Proto Board bundled with 20 pin to 10 pin JTAG adapter cable
http://www.embeddedartists.com/products/lpcxpresso/xpr_value.php


Here are the details:

LPCXpresso Base Board
The LPCXpresso base board is ideal when you need to do prototyping work or when you wish to learn more about the Cortex-M0 and Cortex-M3  microcontrollers. It works with the LPCXpresso boards (LPC1114 and LPC1343) and with the mbed module (LPC1768).The base board is loaded with different peripheral units  with connectivity and inputs that includes an OLED display, accelerometer and light sensors, joystick and connector to optional wireless module.
The network connectivity includes XBee support and ethernet (only mbed), and there’s an SD/MMC card socket and SPI-Flash, I2C port expander and a CAN interface (mbed). The board measures 150 x 180 mm and is powered through a USB connector.  There are also plenty of other things like push-buttons and rotary switch.
To make it very easy to get started, many sample applications have been developed like:

•Rotary switch controls 7-segment display
•Reading and writing to EEPROM
•Joystick controlling LEDs (PCA9532)
•Listing content on a FAT formatted MMC/SD card
•Values from light sensor, temperature sensor, accelerometer and trim potentiometer are written to the OLED display
•Joystick controlling RGB LED
•Speaker - Playing tones
•Speaker - Playing WAV file
•Reading and writing to SPI-Flash
•Reading from UART1 and writing to UART2 (and vice versa)
•Trying to contact an XBee module. Result printed on OLED display
•Values from the BNC is written to the OLED display
•NXP's USB Mass Storage Device example
•NXP's UROM based SB Mass Storage Device example
•NXP's USB HID example
•NXP's ROM based USB HID example
More information about the LPCXpresso Base Boards is found at:
http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php

LPCXpresso Value Pack
Embedded Artists offers an LPCXpresso Value Pack comprising:
•A 10-pin to 20-pin JTAG Adapter designed to convert between the ARM mini-JTAG connector (10-pin) and the standard ARM JTAG connector (20-pin)
•The LPCXpresso Prototype Board with two pin lists and two headers
•A mini-B to A USB Cable
The JTAG adapter lets you connect the LPC-Link to any custom board. The prototype board provides you with an easy-to-use expansion area for your own experiments.

http://www.embeddedartists.com/products/lpcxpresso/xpr_value.php
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Feb 24 01:42:35 MST 2010
Dear Customers,

Code Red has released the LPCXpresso upgrade versions. Starting at $256, they add support for C++, automatic live online updates, Red Trace functionality, Flash utilities, direct support from Code Red and debugging of projects with more than 128KB of code. Please visit http://www.code-red-tech.com/products.php#comparison for a comparison table of the products.

Thank you,
-NXP
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Thu Jan 21 17:22:29 MST 2010
LPCXpresso V3.2 was released on January 21, 2010.

Please visit www.code-red-tech.com/lpcxpresso to download the latest version.

Enhancements:
[LIST]
[*]This version introduces new, faster debugger support for Windows XP machines, and also improves the peripheral views for LPC11xx and LPC13xx devices.
[*]There is an updated example bundle with fixes to the USB examples.
[/LIST]
0 件の賞賛
返信

2,051件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Dec 16 17:44:26 MST 2009
LPCXpresso V3.1 was released on December 15, 2009.

Please visit www.code-red-tech.com/lpcxpresso to download the latest version.

Enhancements:
[LIST]
[*]Added support for LPC11xx family devices
[*]Added checksum utility to create the correct LPC in-circuit programming flash checksum in a binary file
[*]Added a 'Browse the web' button to the Import Examples dialog to simplify searching for new examples
[*]Minor improvements to the Serial Number/Activation process
[/LIST]
Fixes:
[LIST]
[*]Fixed bug with recognizing LPC-Link on non-English language operating systems
[*]Fixed a crash in the LPC-Link debug driver causing a "No error" error when starting a debug session
[*]Fixed issue where another application could prevent the debug driver from connecting to LPC-Link
[/LIST]

Known Issue:
[LIST]
[*]The USB schematic in the included Getting Started guide has mistake. Please download the latest, corrected Getting Started guide at www.nxp.com/lpcxpresso-support
[/LIST]
0 件の賞賛
返信