MSC functions in Rom Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSC functions in Rom Question

597 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ehughes on Sat Feb 12 08:19:20 MST 2011
In the example code for msc_rom there are 2 callbacks for msc_read and msc_write.


It gives an offset and a length.    MSC usb devices are supposed to have standard 512 byte read and writes but I notice that a value of 64 gets passed in alot as the write length.


Is this length parameter constant?   If not how is it calculated in the rom functions?
0 Kudos
Reply
0 Replies