MISRA support Lpc Xpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MISRA support Lpc Xpresso

1,161 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Fri Jul 08 06:10:37 MST 2011
Hi,
I am interested in MISRA rule checking of C code, is this built into LPCxpresso, or are there any plans to do so? I notice this is part of the TI 430 tool set. What do people use for MISRA / lint checking of their code?

Thanks
0 Kudos
Reply
2 Replies

1,103 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jul 09 10:42:55 MST 2011
We have no plans to add MISRA support directly within our tools at this time.

There is some work going on in the area of a static analysis within the Eclipse community as a whole though, which looks like it might become quite interesting in the future - do a google for "codan eclipse".

If you are interested in using Lint, then there is also a far amount of information of using this within Eclipse too (though I've not personally done this). Again try google.

Regards,
CodeRedSupport
0 Kudos
Reply

1,103 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rmteo on Sat Jul 09 06:55:10 MST 2011
AFAIK, no.  For safety and/or mission critical applications, I would look elsewhere.
0 Kudos
Reply