M0 + usb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M0 + usb

2,226件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Apr 12 11:23:28 MST 2011
Hi,
[B]Low Cost Cortex-M0 USB solutions with Smart Card Interface[/B]


I think the only product missing from the NXP-ARM portfolio is ethernet integrated with the physical part. It would save a lot of PCB and money.
0 件の賞賛
返信
9 返答(返信)

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyberstudio on Tue May 31 13:39:47 MST 2011
Is this out yet?
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cyberstudio on Fri Apr 29 12:55:28 MST 2011
Beginning of May? Eagerly waiting for next Monday...
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Thu Apr 14 01:32:09 MST 2011

Quote: whitecoe
Looks like the answer to that is fairly shortly. Press release says...
[INDENT] [I]These devices are currently sampling to lead customers and will be available from distribution worldwide in May 2011[/I]
[/INDENT]http://www.nxp.com/news/content/file_1876.html



Don't we qualify as lead customers?:(  I'll buy 10.:)
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Thu Apr 14 01:25:08 MST 2011

Quote: piperazine
Cool, when/where can i get one? :)



Looks like the answer to that is fairly shortly. Press release says...[INDENT] [I]These devices are currently sampling to lead customers and will be available from distribution worldwide in May 2011[/I]
[/INDENT]http://www.nxp.com/news/content/file_1876.html
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by piperazine on Wed Apr 13 09:16:26 MST 2011

Quote: NXP_Europe
hello piperazine,

board is equipped with an USB-connector.



Cool, when/where can i get one? :)
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Wed Apr 13 04:30:09 MST 2011
hello piperazine,

board is equipped with an USB-connector.

Thansk for the other suggestions.
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by markus_b on Wed Apr 13 02:19:33 MST 2011
I'm missing the analog flexibility of the 8-bit MCU's, there is s lot of room for improvement in this area:
- Vcc range, many AVRs allow 1.8V to 5.5V, saves an external regulator in many projects
- Internal Voltage Reference for the ADC
- Internal differential and gain stages, saves external OP-amps
- Higher current output drivers, 3-4 mA is not much, saves on external drivers

[I]Markus[/I]
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by piperazine on Tue Apr 12 12:09:28 MST 2011
Just been having a look at these too. Also just noticed that there might be an LPCXpresso board with one of these on popping up soon with a USB connector on board. See page 41 of the latest getting started manual.
0 件の賞賛
返信

2,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Tue Apr 12 11:27:34 MST 2011
Now you know why they are Low Cost.:)  You can't have everything on one die, but another chip, sans USB, with ethernet would be nice. 

This is a very nice chip.  Just what I have been looking for.
0 件の賞賛
返信