Lpc812

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lpc812

1,257件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ppx on Mon Jan 07 07:07:08 MST 2013
I have just received a LPC812 board from Embedded Artist. However, I have not seen any posts here that it is supported by LPCXpresso version. Is it? If not, when?

I have also tried to download schematics from www.lpcware.com but the site is down. Are they available somewhere else?
0 件の賞賛
返信
5 返答(返信)

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 07 11:51:18 MST 2013

Quote: ppx
I have also tried to download schematics from www.lpcware.com but the site is down. Are they available somewhere else?



Yes, if lpcware.com server is working you can download schematics here :)

http://www.lpcware.com/sites/default/files/LPCXpresso%20LPC800%20rev%20A.pdf
0 件の賞賛
返信

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 07 10:30:42 MST 2013
It's not the first time (and probably not the last) that EA website doesn't know what EA is selling, it's some kind of tradition already :p

Or they hibernate in a warmer region (together with lpcware website guys) :rolleyes:
0 件の賞賛
返信

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ppx on Mon Jan 07 10:15:56 MST 2013
I know that Embedded Artist should normally have the schematics but they don't.

And I should have searched for lpc8xx instead of lpc800 to find out about LPCXpresso. My fault. :)
0 件の賞賛
返信

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Mon Jan 07 09:46:26 MST 2013
The easy answer is yes - it is supported by LPCXpresso (as of v5.0.12)

And when you receive a board from Embedded Artists would it not be logical to ask them for schematics :eek:. Normally they have schematics for the boards they sell on the website but the lpc812 board is not yet available on the site - I'd just drop them an email and see what happens.

Rob
0 件の賞賛
返信

1,199件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Jan 07 07:35:09 MST 2013
How about this thread?
http://knowledgebase.nxp.com/showthread.php?t=3891
0 件の賞賛
返信