Lpc11e14 eeprom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpc11e14 eeprom

1,909 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Mon Jul 02 09:35:59 MST 2012
Hi,

Does anyone know the address of the EEPROM for this part? I can't find it in the manual.
0 Kudos
Reply
7 Replies

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Sun Aug 26 02:28:27 MST 2012
The link posted by Zero. AN11073
0 Kudos
Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dino on Fri Aug 24 03:36:23 MST 2012
Hi,
I have the same problem with the PLC11U23. How did you fix it?
0 Kudos
Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Tue Jul 03 06:20:05 MST 2012
Thanks zero.

Why can't they put all the information in one place :mad:
0 Kudos
Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jul 02 14:37:21 MST 2012

Quote: OXO
Ah, but those are the ISP return code, not the ISP code which are table 300



I know :rolleyes:

And now make an educated guess: You've found a new feature or this IAP table is an old copy of non EEPROM versions :eek:


Quote: OXO
Any idea on the EEPROM address?



Did you read AN11073 :confused:

http://www.lpcware.com/content/nxpfile/an11073-using-lpc11axx-eeprom-iap-v10
0 Kudos
Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Mon Jul 02 14:02:45 MST 2012
Ah, but those are the ISP return code, not the ISP code which are table 300

Any idea on the EEPROM address?
0 Kudos
Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jul 02 12:00:49 MST 2012
Try:

Quote:

14 ADDR_NOT_MAPPED Address is not mapped in the memory map. Count value is taken in to consideration where applicable.

from Table 287. ISP Return Codes Summary :rolleyes:
0 Kudos
Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Mon Jul 02 10:11:42 MST 2012
Gaaah, and when I try it out with address= 0, the IAP status returned is 14.

But..

UM10518 says status codes on go up to 11. WTF?
0 Kudos
Reply